Gland plates are used with a plinth base to provide cable management solutions while maintaining a NEMA 12 rating. ProLine G2’s unique Duro-Stand Gland Plate was designed to bear the weight of a person, making it easier to work on the enclosure when the gland plate is installed.
ProLine G2 0-mm Solid Bases are used to close the bottom opening on an enclosure frame.
ProLine G2 Plinth Bases install under an enclosure to provide space for cables to enter from below.
No need to use a gland plate in the base of the enclosure with the Fully-Sealed Plinth Base (100mm Solid Base), which includes fully-sealed gland plates on the sides. Solid bases can easily be joined, for convenient cable management in joined/ganged enclosures while maintaining Type 12 environmental rating.
ProLine G2 Disconnect Components are used with ProLine G2 Disconnect Frames and Doors to configure a custom Disconnect Enclosure Solution for widths >1000 mm wide. These components are identical to the standard ProLine G2 components (i.e. ProLine G2 Solid Tops, Gland Plates, Mounting Subpanel) with the exception that the center support is offset 100mm (to accommodate the hinged mullion).
ProLine G2 Transportation Bases provide enhanced stability and forklift provisions for modular enclosures up to a maximum of 3000 mm (118.11) total width in a multiple-bay system.
The ProLine G2 Joining Kit Support Bracket is used in conjunction with the standard joining kit if additional support is desired. The kit includes a quantity of 8, 12 gauge, mild steel brackets with mounting hardware. The brackets span the joined frames and can be placed as needed.
Mobile bases include casters and extend beyond the front and rear of 600- and 800-mm wide modular enclosures to provide enhanced stability.
The Vented Plinth Base Covers replace the traditional solid plinth base covers that mount width-wise across the front and rear of the enclosure. Vented covers allow air to enter the enclosure from below, and are used in conjunction with the Vented Gland Plate. These covers are RAL 9005 black, polyester powder paint, and include all necessary mounting hardware. Please note that a standard 100mm Solid Plinth Base must be ordered separately, as Vented Plinth Base Covers are replacements for the front and rear covers only. Vented Gland Plate also sold separately, but required for successful air passage.
The Plinth Base Mounting Bracket Kit secures to the cast aluminum corner blocks of the standard Plinth Base. The bracket kit serves two functions: the first function is to facilitate floor mounting, and the second is to run a grid network for cable management. Previously, it was challenging to secure an enclosure to the floor, but with the bracket kit the mounting holes are now easily accessible from inside the cabinet after gland plate removal. Grid straps can also now be mounted to the Plinth Base Mounting Bracket Kit to secure cables entering or leaving the cabinet through the base. Grid Straps and Plinth Base are sold separately. The brackets are constructed from a 10-gauge (3.0 mm) steel, and finished in RAL 9005, matte black.
The Floor Stand Kit mounts depth-wise on the ProLine G2 enclosure, securing both through the frames drain hole(s) and the corner block(s). The Floor Stand Kit is used to elevate the enclosure off the ground by 300 mm (~1ft). The stands are constructed from a 12-gauge (2.5 mm) steel, and finished in RAL 7035, textured light gray. Please note that at this time Hoffman is only offering a single 800 mm deep model, please consult the factory if a different depth is required.
Connect With Us