Skip to main content

Please Select Your Country/Language Preferences

For trouble-free operation of the air/liquid heat exchanger the quality requirements of the coolant must be maintained; The selection of appropriate anti-corrosion and frost protection agents depends on the environment in which the unit is used and on the external chiller (VDI 3803, see also user manual).
At coolant temperatures below 14 °C, there is an increased risk of condensation. We recommend requesting a customized unit with integrated condensate management.